This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24210: single cell li-ion battery and Solar panel (6V, 2W)

Part Number: BQ24210
Other Parts Discussed in Thread: BQ24650

Hi everybody!

I'm thinking of use the BQ24210 to charge a single cell li-ion battery from a solar panel (6V, 2W), however i have some doubts about it. As far as i understand, the BQ24210 does not have a battery protection circuitry. For example, under voltage protection of the battery is not implemented. So, I thing I need to use some extra battery protection. Bottom line, I'm looking for an IC or more that are capable of charging one single cell li-ion battery from a 6V solar panel and protect the battery. My final power managment circuitry must be able to deliver 2A pulses to the load. Do you have any suggestion?
Thank you for you help.

Miguel