This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am Using 4 nos of TPS54526 in my design. 5V is the input to all the regulators & outputs are 3.3V, 1.8V, 1.5V & 0.95V. Inductor value is given in the datasheet for output voltages from 1V to 5V. Can I use 1.5uH Inductor for 0.95V output?
Best regards,
Bhagavath