This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQPRODUCTION: HPA495 seal after programming dynamic pack data

Part Number: BQPRODUCTION
Other Parts Discussed in Thread: BQ40Z50, , BQ28Z610, BQSTUDIO

Dear E2E-Community, 

I'm programming Bq28z610 and Bq40z50 with goldenfiles via a HPA495 in BQPRODUCTION, but I'd like to know, if there is any way to seal the device, after dynamic pack data has been programmed, 

If It's sealed within the golden file, then bqproduction is not able to programm dynamic pack data into the device. Is it possible to send the seal command, via EV2300 + HPA495, without starting BQStudio?... It would really improve the production, when there is no need to start a 2nd Program.... 

Best Regards and thanks in advance, 

Felix