I'm not able to have the bq2010 gas gauge "learn" new battery capacity. This is an old gauge and I wouldn't use it now but having issues with battery packs in the field.
Scenario: say CPI is 3 (three times charged without a qualified discharge), when I charge the battery the LMD seems to always get to PFC-1 (or perhaps as I put the battery to use and read registers one count goes down), then I discharge the battery to below EVD1, however, CPI does not reset to 0-stays at 3. This leads me to believe that re-calibration didn't take place.
Please advise.