Hi,
I'm using TPS61193-Q1 and I define the maximum output voltage is 24V through R1 and R2. In the datasheet, it states that "Recommended maximum voltage is about 30% higher than maximum LED string voltage" in 8.3.1 chapter.
My question are:
1. How to estimate the 30% above the maximum output voltage? Can we get 50% or more higher?
2. When we apply the maximum voltage 24V, it will shut the output voltage after about 550ms. How to define the lasting time?
Thanks.
Kevin Xiong