This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24075-Q1: Efficiency and other questions

Part Number: BQ24075-Q1

Hi. 

The device we are designing has a LiPo battery and we are looking for the charger that suits best for our purposes.

We pretend to charge the battery at 1.2 - 1.5 A so we are focus now on BQ24075-Q1, that seems that fits our needs.

I have read that when this device is only operate with battery there is a drop of 50 - 100 mV on the OUT vs the battery voltage. Since our device is portable and a long battery life is a key feature, is it relevant this dropout in terms of efficiency? The current along our device is about 25-35 mA.

If BQ24075-Q1 is not the best battery charger for our device, can you recommend us another one? The only requirements are to be able to charge the battery at 1.5 A and the lowest power consumption possible when the device is running only with battery. 

Thank you.