Team,
Please help address customer's questions:
- On the LM76003, there is a note that the SYNC/MODE pin can be connected to either Ground (DCM/PFM mode) or “Logic High” (force FPWM mode). What is the proper connection for “Logic High”? Is this just routed back to the output voltage of the LM76003?
- The CBIAS cap is connected with pin 9 BIAS. Its value is 0.1uF in evaluation board. But the value is recommended 1uF in LM76003’s data sheet page 4. Which one is correct?
- The value of decoupling CAP is used 0.47uF for input pins PVIN in evaluation board. But the value is recommended 47nF in LM76003’s data sheet page 27. Which one is correct?
Thanks
Viktorija