This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55165Q1-EVM: ask about Working current.

Part Number: TPS55165Q1-EVM


Hi there.

I test with TPS55165Q1-EVM.

Here is default setting.

1. VIN : 12V

2. VOUT : 5V

I checked current consumption with no load condition.

1. IGN OFF (shutdown), No Load : current consumption near 3uA, It meet datasheet.

2. IGN ON (Normal mode), No load : current consumption up to 16mA

  * I thing and under this condition is idle status then 16mA current consumption is more than high what I think.

  * So I try to find current consumption of normal mode & no load condition, but I can't.

3. IGN ON (Low poer mode), No Load : current consumption near 17uA, It acceptable and meet with datasheet.

So I wonder... why normal mode operation with no load condition use around 16mA current consumption.

Any advice is thanks.

Good day.