I have the bq27x10EVM wired to the EV2300 I2C USB communications unit and the software loaded and operational.
Thing is, I don't understand the process of evaluating the bq27210 part using it.
I am using a 5000maH LiPoly battery. I have an electronic load and a charger available for connection.
I am not sure what the next steps are.
I expect to see this all show realtime life of the battery given the discharge rate set by my electronic load.
I read that there is a calibration mode but see no instructions really on what to do.
I am also concerned that perhaps this all will not function correctly with a battery with this high of mAH.
Perhaps I need to rewrite registers in the EEprom. Need someone to talk me though this a bit.
Barry 949-672-7602