This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55165-Q1: Ask about wake-up condition or operating range of TPS55165-Q1

Part Number: TPS55165-Q1


Hi there.

I choose TPS55165 for my main DCDC.

1st) Low Iq

2nd) Wide input range

3rd) Buck & Boost

I make sample PCB with TPS55165-Q1. Vout is fixed 5V.

I have some problem about Input range or wake-up. I'm not sure this is wake-up problem or input range it.

Anyway, I test about input range from 3V to 12V.

In wake-up condition, 7.5V or higher is fine.

Fine means Vout 5V is OK.

But lower then 7V case is bad.

Bad means no Vout(5V).

Use IGN pin only.  (No use of IGN_PWRL, so tied to GND with IGN_PWRL)

From the datasheet, min VIN voltage is 2V (VOS_FB tied to GND condition)

I want to use Buck-Boost mode freely.

Input range from 3V to 20V. 

Current output up to 300mA is fine.

In this condition, TPS55165 is very good solution I think. But it operate is not good until now.

Please give to me any advice to use happily  TPS55165.

Thanks.

BR.

  • Dear Sir,

    2V is the UVL voltage, not the startup voltage. The startup voltage is much higher than 2V, which should be at least  >5.3V min.

  • Dear Helen.

    Thanks for your reply.

    From your datasheet about TPS5516x-Q1.

    1. Features

      * 2-V to 36-V Input Voltage Range for Vout = 5V

      * 1-A Output Current for Vout = 5V and Vin > 5.3V

      * 0.8-A Output Current for Vout = 5V and Vin > 3.8V

      * 0.4-A Output Current for Vout =5V and Vin > 2.3V

      * Automatic Transition Between Step-Down and Step-Up Mode.

    From the "Features"  which I write upper.. set Vout = 5V and Current Limit 0.4-A condition... and also Automatic transition Buck & Boost.

    So with my condition..(0.4A & 5V).. then I can use input voltage range from 2.3V to 36V.

    For actual use... Can I use input voltage from around 4V to 16V, and 0.3-A Current load???

    If my understanding is wrong... please let me know about it.

    Thnanks.

    BR.

    CHANYOUNG.

  • Hi Sir,

    TPS55165 can support 4-16Vin, Io=0.3A. But make sure the start up voltage is high enough, at least> 5.3V After startup, the Vin can be tune to a very low value.