Other Parts Discussed in Thread: GPCCHEM
In my 1S2P battery pack Qmax drops with each discharge cycle and the cell voltage for 0 % SoC rises in small steps from 2.7 V for new cells to 3.3 V after a few cycles. The full charge capacity and the runtime of the device powered by the battery pack also drops continuously.
My parameters are:
designVoltage 3700, terminateVoltage 2500, reserveCapacity 200, designCapacity_mAh 6700, designEnergy 24790, taperRate 240 (=280 mA), dsgCurrentTh 700 (=95 mA), chgCurrentTh 700 (=95 mA), quitCurrent 1000 (=67 mA), simRate 0x219 (280 - 3350 mA), loadMode 3 (constant current, average of 14s)
I charge with up to 2 A and discharge with 5 W. My microcontroller stops discharging at 0 % SoC. I wait 2 h when full and 2 h when empty so that Qmax is recalculated.
Why do I 'loose' battery capacity?