Part Number: TPS62172
Other Parts Discussed in Thread: TPS62130, TPS62147
I’m planning to use TPS62172 to supply 3.3 V to a load that will vary between ~100 mA and ~350 mA. Referring to Table 1 in the app note, Optimizing the TPS62130/40/50/60/70 Output Filter, I see that the converter should be stable with a 10-uH inductor and an output capacitor no larger than 22 uF. I’d like to use 10 uH to keep the converter in continuous conduction mode.
With respect to that 22-uF limit, to what extent do I need to consider the distributed capacitance of my board—all of the decoupling caps, as well as the capacitance between power and ground planes?
Also, Table 1 indicates that “effective” capacitance is one-half of the nominal capacitance. Is that a reference to the voltage coefficient of capacitance of (non-COG) ceramic caps?
Thanks for any insights you can give me...