Other Parts Discussed in Thread: CSD, TPS53626
Hi BU,
Can I use TPS53622 x1 and CSD 95377 x2 to design of VCCIO(Imax 44A) in VR13HC? If I wanna use CSD 95377 to design VCCIO, which multi phase V-core controller can use?
Jet
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, TPS53622 is not compatible with that power stage because it does not support DCR current sensing. Instead I would suggest either using the TPS53626 controller, or transitioning to a power stage with integrated current sensing.