This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO5452: SIC short circuit protection

Part Number: ISO5452


Hi

I'm developing a motor controller using the ISO5452 as the gatedriver controling a SIC mosfet with a Ron of 0.03 ohm

I'm looking into how to decrease the current that the gatedriver shuts down on, the circuit looks like this:

diode with Vf of 1.3-2 V in series with a resistor R, following the design suggestion in the datasheet

To avoid a redesign I need a solution which either adds a diode with larger forward voltage or increases the resistor value R

I'm looking for a solution where the gate driver shuts down at approx 80 A, giving the following calculation

(9V- Vf-80*Ron)/500uA = [8900 10300] ohm for R

Is this calculation correct, can I just increase the resistor R or is there another way to achieve the short circuit protection?