This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25713 : Please recommend charging circuit and monitor circuit.

Part Number: BQ25713
Other Parts Discussed in Thread: BQ24610EVM,

hello

I tested the charging circuit with bq24610EVM.
There is an issue with pre-design monitoring
BQ24713 is under review.
I am worried about whether I can review it well.
request for Altium EVM layout source files


Currently reviewed specifications

1. The product is charged using an external adapter.
2. Use only the power check of the battery.


Li-ion 3S1P
Charging voltage 12.6V
Charge current limit 1500mA
Charging 15V / 2A Adapter
Communication using I2C