Other Parts Discussed in Thread: UCC28951, UCC28950, UCC21521
Hello
I'm designing dc dc converter of 1.32KW for battery charging.
specifications : Vin 310-410VDC
vout 13.2 V and 100A
Here are the schematics of power circuit and control circuitcontrol circuit edited new.pdf
1) we have designed for 100A output and initially we are testing for 13.2V and 25A output.
RRE and RS in the control circuit schematic is 7.2k and 72 ohms respectively(for 25A testing) and for 100A we got 2.2k and 22 ohms. actual calculated values of CZ ,CP , and RF are 8.54nF ,854pF and 18.6Kilo ohm respectively. and we implemented the control circuit as in the schematics and other changes we made except those values.
2) We gradually increased the input dc voltage from 0. we have seen the output voltage and current is also increasing significantly. At 290Vdc input, we got 13.2 V and 1A (10 ohm resistive load at output) at the ouput.But we have not reached to our operating range i.e 310V - 410V , we increased the voltage to 300 , the output started fluctuating between 0 V to 14V . stiill we increased to 310,now the mosfets (QB,QC, QD) had blown out.We had seen it for two times happening the same at that voltage and above.
we have taken mosfets(QA,B,C,D) rating 1000V,35A .
what might be the issue and problem?
help us
Thanks and regards
rajashekar