Other Parts Discussed in Thread: TPS2373, TPS2373-4EVM-758, , PMP20541
Hi
Currently, my client is trying to develop POE by applying TPS2373 and UCC2897A based on TPS2373-4EVM-758.
I was very satisfied with the EVM.
But it is too expensive to apply UCC2897A as active clamp circuit.
So we want to apply UCC2897A as flyback.
There are some questions about the application.
1. I would like to know about the setting of the AUX stage if the 2nd SR IC is not applied.
2. The datasheet only shows the ovp for the input. Can I make OVP settings for the output?
3. It has been confirmed that there is very little inrush current when it is active clamp. Can Flyback get the same results?
please answer about my question.