I am using two TPS65950 companion devices to power OMAP 3530 processors in my design.
The design and layout of both TPS65950 companion devices (functional and non-functional) are almost identical. The functional TPS65950 companion device does not have its ULPI and Keyboard interface connected.
When I touch the probe to VREF pin, its output starts decaying from around 500 mV to 100 mV over 10 seconds. When I remove the scope probe from the pin, it VREF again goes up sets around 400 mV.
32-KHz tuning fork crystal for that companion device didn’t work. I tried removing 22pf ceramic capacitors as well.Therefore I connected 32.768 KHz, 1V Amplitude clock from the function generator to 32KCLKIN pin of the companion device. It still has not changed situation.
I also checked VINTANA1 LDO output of the companion device. It is zero as against 1.5V, expected value. My understanding is VINTANA1 should come up irrespective of 32KHz clock is available or not.
I would appreciate if anybody could please provide more insight.
Thanks,
Shashank