Tool/software: WEBENCH® Design Tools
Is it possible to use Webench to design multiple output dc-dc converters? I am trying to use it for a converter that requires 12 V, 5 A, and 5 V, 6 A outputs. The input voltage range is 30 V to 100 V. Whenever I try to input this data, there is no option for a second output. So, if you have multiple output dc-dc converter you can't use Webench, correct?
Thanks,
Chuck