Hello again;
I need clarification: I noted that the datasheet says (8.3.1) that by default (from factory), all analog faults (UV/OV) are disabled. However, the FO_CTRL register's default value is listed as FFFC, meaning that both these faults are "enabled"??
However, since the CELL_UV threshold register defaults to 0000, and the CELL_OV threshold register defaults to FFFC, do I "assume" correctly that these out-of-range values are doing the effective "disabling" of these faults?
Thanks in advance.