hi, I'm doing a design to power up a raspberry from battery, so I'm using the BQ24618 to recharge the battery, I'm seen a typical application on the datasheet and it recommends a Diode in the adapter input (D5 in the picture) but I don't see a reference, could you tell me the requirements for this diode my system configuration will be :
The raspberry has a heavy algorithm with large power consumption about 1.6A on average with peaks of 2.5A with all the peripherals
VIN=5V, 1-Cell, IAdapter_limit = 4A, Icharge = 1A, Iprech=Iterm=0.3A,
and the reference for de MOSFETs Q4 and Q5 are not available, there is a mistake? can you help me to find the datasheet or a similar reference to use
Image of the reference design
RED = diode
BLUE = MOSFETs
Thanks.
Rafael Rodriguez