Other Parts Discussed in Thread: TPS92515
hi
in my design i require to sync the flash signal of the camera with the LEDs,
and i have a 5%-10% duty cycle for the LEDS,
can i use the PWM signal as a GPIO to toggle the signal up/down to turn on the leds, or do i need to add an external FET after the inductor to control the on/off of the leds?
i have two rows of 3 leds each, each row is ~9.6@1A
thanks for your reply
Tzachi