Other Parts Discussed in Thread: UCC28950, SM72295, SM72442
Hi
Currently my customers are developing 600W class solar converters using SM72445 and UCC28950.
The configuration is as follows.
There are many difficulties in designing circuits based on EVM.
Is the SM72445 capable of buck / Boost 600W design with 48V output?
Is there a document I can refer to if it is possible, or should I review the data sheet only?
If not, will there be alternatives available for MPPT Control?