Hi Ereryone,
Can i use EADC to instead of ADC? Can you show me how to config the EADC , thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
It's true that both are SAR. In fact, the EADC is faster - 6 bits at 64 ns, which the ADC is much slower - 12 bits at 3.9 microseconds.
But the EADCs 6 bits only cover a maximum of 512 millivolts range.
The SAR mode on the front end uses the EADC SAR and the EADCDAC, plus some logic, to make a SAR convertor which covers the full 1.6 volt range of the EADC DAC. I have been told that it's actually faster than the ADC, taking about 2 microseconds to complete, typically.