Other Parts Discussed in Thread: TPS92515, TPS92641, LM3409
Hi
Currently, our customers are developing the following LED Module using TPS92512.
Vin: 41Vdc, Load: 12 lines Serial (3x12 = 36V)
PWM dimming is changing LED brightness and color temperature.
However, if the PWM frequency is set to 6kHz or less, the LED brightness and color temperature change normally, but audible noise is generated.
If the PWM frequency is set to 20kHz or higher, audible noise will disappear.
However, the LED blinks at certain intervals.
The actual PWM Dimming frequency is 20kH.
From the datasheet, most of them seem to be designed to be less than 1kH at 250Hz.
Could the corresponding PWM frequency be a problem?
Is there anything I need to review? Or can you recommend another IC?