Other Parts Discussed in Thread: TPS2372, PMP20859, TPS2378
Dear Team,
My customer wants to use TPS23754 for two RJ45 port for the redundant application.
Here is some question from the customer:
1. If both of the RJ45 port supply power will cause a short circuit or handshaking issue?
What is the issue need to be careful with two RJ45 port?
2. Can we setup priority for two RJ45 port?
3. If one of the RJ45 remove, can another port suppourt directly?
Both Ethernet ports must support 802.3at PD with automatic failover with zero downtime.
BR
Kevin