Hi
My Customer has question.
Can I use only the current sink function without using the Boost function of LP 8860-Q1?
The simple configuration is as attached.
Best Regard
T Kishi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
My Customer has question.
Can I use only the current sink function without using the Boost function of LP 8860-Q1?
The simple configuration is as attached.
Best Regard
T Kishi
Hi, Shirley,
This is *almost* the application I want to ask about. I want to use one LP8860-Q1 without any boost power supply:
The application is to control a set of LEDs (4 strings of 3 diodes each), using only the precision current sinks ( 0 to <65mA), with a fixed (~12VDC) power supply.
No external PWM, just SPI or I2C.
If my circuit leaves out all of the boost topology parts, what do I need to do to operate the LP8860?
* Supply 12VDC at Vdd
* Connect VSENSE_P to VSENSE_N
* Connect FB to +12V ??
Can I leave out C2x and Ccpump ?
What about Isense and Isense_gnd ?
Anything else to worry about?
Initially, what do you recommend I do to test this all out using an LP8860-Q1EVM eval board?
Thank you!
Dave
Thank you, Shirley!
To make sure I understand correctly,
What about Isense and Isense_gnd ?
Connect ISENSE to ground.
Connect both Isense and Isense_gnd pins to power/analog ground?
Can I leave out C2x and Ccpump ?
Be sure to disable the charge pump.
Is there an Enable/Disable pin I missed, or do I disable via SPI/I2C?
Be sure to disable all the fault detections of the boost or make sure the faults cannot be triggered.
Similarly, via SPI/I2C, or ae there hardware Disables?
Dave