Other Parts Discussed in Thread: TPS22990
Hi,
We use the TPS6590379 in one of our designs. Now we checked the OFF2ACT sequence against the data in the User's Guide (sliu011f, page 15).
We can see that the time between SMPS7 and SMPS12 is approximately the 550us (please see picture 1).
But when we measure the time between REGEN1 signal and RESET_OUT signal we have 1524us versus 1100us (please see picture 2) and time between REGEN1 and LDOUSB is 918us versus 550us (please see picture 3).
We use an external switch (TPS22990) that is switched on with REGEN1 to switch on the 3.3V main rail.
Is there an error in timing of the User's Guide? If not, what could be the problem in our design?
Thanks and best regards,
Patrick
Picture 1: SMPS7 on CH4, SMPS12 on CH3
Picture 2: REGEN1 on CH4, RESET_OUT on CH3, 3.3V main rail on CH1
Picture 3: REGEN1 on CH4, LDOUSB on CH3, 3.3V main rail on CH1