Dear Team,
here is a question regarding the startup current tolerance of UCC28910. The datasheet shows the following:
As the start up current source is charging the Cap on the VCC pin it defines the start up time. The datasheet shows a quite big variation of 1:10 for ICH2 and ICH3. Does this really mean the start up time can vary by a factor of 1:10? This seems to be quite large.
Fig. 16 shows the temp dependency with a factor of 1:2.
I guess the parameter in the above chart also includes process variation. However why is the variation so huge?
thanks
Lutz