This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28911: Calculation of Transformer Turns Ratio

Part Number: UCC28911


Dear Specialists,

My customer is considering UCC28911 and has a question about transformer design.

I would be grateful if you could advise.

---

I am designing transformer by datasheet 10.2.1.2.3 .

When Dmax=0.482, Vbulk(min)=80V, Kcc=0.413, Vocv(vout)=24V, VF=0.35V

Calculated Nps became 3.83 and Npa became 1.2.   

In this case, What value should be used?

In the datasheet, Nps value is recommended for 5V, but not for 24V. 

---

I appreciate your great help in advance.

Best regards,

Shinichi