Other Parts Discussed in Thread: TPS706
Hi,
in LP5910 datasheet.
1. I wonder -20uA means the current flow out from IN or into IN is 20uA?
2. My customer is using some competitor's device which, when input is unconnected and output connected to 3.3V source, they will observe 3.3V at input side. They don't want the output voltage appear at the input side. So they will need reverse current protection LDO, right? Or reverse voltage protection?
3. How is reverse current protection achieved?