This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2549-Q1: control pin configuration with microcontroller

Part Number: TPS2549-Q1

Hi,

I would like to know if I can use microcontroller to control the CTLx pins instead of hardwire them?

I want to configure this device in such a way that it has the flexiblity to detect the plugging device

For example, when user plug in USB flash drive for playback purpose , the DP_out and DM_out will tell the MCU to set the CTLx to CDP/SDP

whereas when it require to charge with 2.1A, MCU will configure it to DCP and stop transmitting data

Is this device capable to do so?

Thanks