Other Parts Discussed in Thread: PMP8861
Can UCC24612 work in Active clamp forward SR,
Can I provide a reference design?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Thank you for your interest in UCC24612.
You can use UCC24612 in a Active clamp forward topology, the thing to look out for is the switching frequency of the SR controller. UCC24612 should be used for <100kHz in a forward topology if you increase the frequency its turn-OFF speed may become a concern which will affect the power losses across the device. In a forward topology there is some current always present in the output inductor, sometimes this current will be large enough to prevent the SR-FET from turning off when the converter is transitioning from freewheeling to power delivering state (turn-OFF threshold is -10mV). This could result in an overshoot resulting in damaging the SR-FET.
I would suggest using a self-driven SR-FET or a gate drive transformer, which is a better option for a forward topology. Attache below is PMP8861, it is a good starting point.

Regards,
Sonal