1) We are using BQ5100YFPR with PMIC BQ25120YFF and the I2C communication/configuration doesn't work if we just use the Battery input for supplying the IC.
2) During the WCH I get some Faults which I could not assign to any possible cause (UV, OV, OL).
the Registers are as below:
C1-0F-AF-60-0E-78-B2-FC-68-0A-00-42
3)If I switch during WCH to battery mode the PMIC config stays valid but the I2C communication doesnt work anymore.