Other Parts Discussed in Thread: GPCCHEM
Hi Friends
I have some doubts regarding the following
1) Can we configure or is that a valid method of changing the guage cc_gain and configure the 8000mAh capacity to 10000mAh fuel guage.
2) I am able to detect the insertion and removal of battery by reading the flag register. And after that I am configuring the guage capacity according to my battery specs which is 10000mAh.
But when battery charger voltage is present and at that time if I remove and insert the battery and after the configuration then battery's remaining capacity and full charge capacity will be same. I don't have any reference schematic to check if their is any problem with my schematic.
Regards
Harish