Other Parts Discussed in Thread: UCC28950EVM-442
hello Sir
I have designed Control circuit for Dc dc converter of rating 1320W
Input specifications of dc dc converter 310Vdc - 410Vdc
Output : 13.2V ,100A
Here im attaching Control circuitControl circuit edited new 1.pdf
ADEL and ADELEF pins get fixed voltage through resistor divider which is from Vref (constant). So there is no change in the delays as input varies.
1) If i have to change and have the feature to change the delay between each leg switches on the primary side of transformer , I should connect it to the CS pin .Am i right ?
how should i calculate those resistor values ( REFHI ,RAEF ,RAHI ,RAHL ) such that delay will change accordingly as input changes.? what is the procedure to calculate them ?
Please help
Thanks and regards
Rajashekar