Other Parts Discussed in Thread: BQ25700
The OTG operation can be enabled, the conditions include:
VBUS is below VVBS_UVLO;
The questions are:
1. VVBS_UVLO can be set by register or not? if can, which register?
2. Normal input voltage is 12V, if input voltage drops to 9V, higher than VVBS_UVLO falling threshold 2.4V, EN_OTG is invalid????? How can I enable OTG when VBUS drops to 9V?
wish your reply ASAP, the project is urgent, thanks
BR
Jelly