From my understanding this board only monitors and balances the cells connected to it but does not charge the cells is this correct? If it is then I would greatly appreciate it if anyone could provide any sugestions/guides/block diagrams to how charging multiple cells would work in this case. Do we simply need a power supply or some kind of special charging device? How would the device connect to the BMS to work in tandem? For reference our team is currently working with around two 48s cell configuration so we would have 6 total of the boards.
Any help is greatly appreciated.