This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63000: If TPS63000 Vin change to USB input supply

Part Number: TPS63000


Dear,


our client RFQ TPS63000, if our desgin is input USB 5V, it`s could be workable?

 

condition A: battery input Voltage Range is 2.7V to 4.2V , Vo/Io= 3.3V/1A

condition B: input 5V USB


if any suggestion, Please advise me.


Thanks,


Best regards,


Lawrence.