This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24133: STAT output - is there an internal pullup?

Part Number: BQ24133

In the datasheet, Pin Functions table (section 7, page 5), STAT pin says "Open-drain charge status pin with 10-kΩ pullup to power rail."

Is there an internal pullup?

If so, to which power rail?

Section 9.2 Functional Block Diagram shows no internal pullup.

I wish to connect STAT pin to an MCU with 3.3V I/O, configuring this I/O as input with pullup (to the MCU's 3.3V). I want to make sure there isn't another pullup to a higher voltage rail that might stress the MCU input.