This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62065: If TJ(junction temperature) has a margin on the d/s

Part Number: TPS62065


Hi team,

Recently my customer UAES has a question about the TJ, They want to know if there's some margin left for the maximum value of TJ(125℃).

Because they want to do a test under the condition of ambient temp=85℃. So they have some concerns about the maximum TJ value. Through the Webench simulation we found the IC temperature is 105℃, but customer did not believe the simulation result.

So could you please tell us if the TJ maximum value has a margin ?

Thanks a lot

Best regards

Jessica