Hello TI,
I actually want to use Module BQ51021 for our application as power receiver in wireless mode only. There is not required to usedUSB adpater as an external supply. Therefore, AD pin can be set on GND. Yes?
another question is regarding pins: WPG and PD_DET. These pins are Open drain output. Should these pins be remained floated (free, NC) or it must be connected? If it must be connected, with whom and how? I don't want to use I²C and therefore SCL,SDA should be connetcted to GND.
Please give me brief info regarding these pins connection on Hardware side.