Hi Support team,
I have a customer using the tps63070 in a design and am having an issue with start up. The device is on a 500mA USB ckt and is drawing too much current on start up. Is there a way to slow down the start up ramp, or delay the start up?
I can send schematic via email. Noticed input caps are only 10u f not the 30 uf recommended.
Thanks
Jeff Coletti