Other Parts Discussed in Thread: BQ76200, BQ78350, BQ24610, , BQ78350-R1
I use bq78350 + bq7692000 + bq76200 and the high-side driving method to immplemented my design.
I use a 5S1P pack. My charger is bq24610.
When I discharge the batttery to 8V,the module can't provide a output voltage, and my charger can't charge the battery.
I have to press the boot button connected to pin TS1 of bq76920 to charge the battery.
When I discharge the batttery to lower voltages , pressing the boot button connected to pin TS1 of bq76920 can't charge the battery.
I didn't use the circuit used in the document -tidrqy7. And I did't use pack monitor function of bq76200.
I want to know if I discharge a battery pack to a lower voltage ,say 1V, what I should to do to charge such a deeply discharged battery?
Can I implement my purpose symply using the circuit in the in the document -tidrqy7?