Other Parts Discussed in Thread: BQ51013, , BQ25100, BQ51003
I'm working on a small wearable project where PCB area is very precious and we'd prefer a one-chip solution vs. two-chip solution. Battery is a coin cell with nominal charge current of 40mA. I saw that the BQ51050B isn't recommended for charge currents below 500mA so we would need to go with a bq51013 + charge IC. Can we do this with the bq51050? Is it that the current regulation is poor below 500mA, or is there another reason?
Also, if you're working on the product line I recommend having a version that supports low charge currents and/or that incorporates a low-Iq buck converter too to reduce component count.