Part Number: TPS62162-Q1
Hi All,
How to understand the enable threshold of TPS62162-Q1, why the VEN_H min value is smaller than the typ value, and the VEN_L max value is smaller than typ value?
Does this mean that typically 0.6V can turn on most of the device, and 0.9V can 100% turn on all the devices? and 0.3V can 100% turn off the devices?
Best Regards
Charles Zhang