This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS560430: TPS560430YF webench simulation question

Part Number: TPS560430


Hi 

We are running Webench using TPS560430YF  to run Webench. 

With below condition Vin : 8 ~ 36V, Vo :3.3V, Io : 600mA(max), Fsw : 2.1MHz,. the webench can not come out a result. 

Can you help us understand what is the issue? 

Also if we are using TPS560430YF , under this condition Vin : 8 ~ 36V, Vo :3.3V, Io : 600mA(max), will TPS560430YF  be stable? 

Thanks!

PY Tsai