Hi
I am working on a step down converter using PSFB topology. The IC ucc28951q1 suits my purpose. My initial work of designing control card is completed. Now when i try to test the control card i observe these following
1. I observe gate pulses on channel A, B, C & D with around 50% duty cycle. My question is will these gate pulses appear even if there are no feedbacks ( output voltage and input current)?
2 . When I externaly give DC supply to pin 3 through a voltage divider and triangular wave with 2V peak amplitude and frequency being my switching frequency, I am not observing any changes in the duty cycle. Also if I fiddle with these external signals I expect my duty cycle to vary, but I am not observing any changes. I want to know If I am going wrong in testing the control card, or there is any mistake in my calculations?
I refered 600W PSFB DC-DC converter for my design