This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61197: Question about output capability

Part Number: TPS61197
We want to use the TPS61197 to drive an LCD panel backlight. The parameters are:
Input voltage: 12V
Output voltage: 37V
Output current: 550mA
The application is fairly demanding, so I need to know that operation at these levels will not cause undue stress. If the TPS61197 is not suitable, what would you suggest as a substitute?