This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM76002: Usibg inducor of LM76002

Part Number: LM76002


Hi

Pluese let me ask you about inductor of LM76002.
My customer will use LM76002 the following condition.
But they will use NS12575T330MN as inductor because it is cheaper than the inductor of 10uF.
Can they use this inductor with LM76002?

 Vin:48V or 27V
 Vout:3.3V
 Iout:1A
 Fsw:300kHz

 Inductor:NS12575T330MN

Best regards,
Yokota